11/2/2020 1:40 AM | |
Posts: 9 Rating: (0) |
That would be great if someone could look at this project. I think I uploaded the plc into the project properly. AttachmentProject4.zip (229 Downloads) |
11/2/2020 2:26 AM | |
Posts: 9 Rating: (0) |
|
11/2/2020 6:30 PM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating: (173) |
Attached are snapshots and extracts of the program and manual. See if it helps and if I missed something experts on the forum or siemens support should be able to pick it out. Edit: I updated the attachment to include setting for telegram time off. Attachmenttreadmill_.zip (245 Downloads) |
Last edited by: Kal.A at: 11/02/2020 21:21:47Last edited by: Kal.A at: 11/02/2020 21:22:12 |
|
This contribution was helpful to2 thankful Users |
Follow us on