5/10/2024 1:22 AM | |
Joined: 3/29/2023 Last visit: 9/25/2024 Posts: 2 Rating: (0) |
I tried S7-PLCSIM Advanced in distributed communication as the pictures. I set the computer ethernet adapter and PLC instance to the same network. As computer and PLC instance connected to the virtual switch as described in the picture, but I could not ping the instance from computer until I set the Siemens PLCSIM Virtual Ethernet adapter to the same network. It does not make sense because computer and PLC instance are already connected to the same virtual switch, why do they need the virtual ethernet adapter? or did I do something wrong? (I can ping to a real PLC connected to a real switch) ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/10/2024 08:27:39New subject after splitting |
|
5/10/2024 1:27 AM | |
Joined: 3/29/2023 Last visit: 9/25/2024 Posts: 2 Rating: (0) |
This picture is how I set the real adapter, and a instance I made |
Follow us on