1/16/2017 11:05 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980) |
Hello, which PLCSIM Version, Which Operation System? Christoph |
1/16/2017 12:34 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi Dinesh KJ, When you install a certain PCS7 version, you cannot use any other service packs of the Simatic family unless it is released. Always check the compatibility with PCS7 not with Simatic Manager or WinCC or any other component. PCS7 is composed of several Simatic programs. PLCSIM is included with the PCS7 DVD's, so install it from the PCS7 DVD. Then you know it is released. Which version of PCS7 are you using? To use PLCSIM 5.4 SP4, you need at least PCS7 v7.1.
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
1/16/2017 12:45 PM | |
Joined: 1/24/2013 Last visit: 7/19/2022 Posts: 226 Rating: (42) |
Hi, Good information, Am using PCS7 version V8.0 Upd1. -- Thanks Dinesh K |
1/19/2017 11:05 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Nice! |
If I could help you, you can use the RATE button. Thank you. |
|
12/21/2017 1:17 PM | |
Joined: 6/19/2017 Last visit: 4/26/2024 Posts: 7952 Rating: (162) |
New question published by bassemalobaidy is split to a separate thread with the subject Can't install S7-PLCSIM V5.4 incl.sp3 in laptop windows 8.1. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on