5/26/2014 3:03 PM | |
Posts: 133 Rating: (0) |
Hello, I have S7-PLCSIM open and in stop mode. When i load CPU blocks, it is said "connection to communication server is interrupted" help me, thanks!!
|
5/26/2014 3:18 PM | |
Joined: 8/27/2010 Last visit: 4/13/2024 Posts: 417 Rating: (37) |
Over which interface you are connected to plcsim? Can you check set pg/pc interface option?
|
5/26/2014 3:25 PM | |
Posts: 133 Rating: (0) |
it is over Profibus, the PG/PC inerface is set to PLCSIM.PROFIBUS.1 |
5/26/2014 11:29 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (272) |
Hello, Please have a look at following FAQ might help you. How do you test the I/O using the S7-PLCSIM simulation program? Video Tutorial to get started with S7-PLCSIM |
VANDE MATARAM..... |
|
This contribution was helpful to1 thankful Users |
5/26/2014 11:51 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (272) |
Hello, Have you gone through above FAQ? Please find manual for more details. You can also check the diagnostic buffer info. 1) Goto PLC---> Module information (ctrl-D) tab diagnostic buffer. you cansee theerror message and the error OB in the diagnostic info. Downloading an Error OBwill stop RED Led Blinking. AttachmentC:\Amit\Maunal.pdf (237 Downloads) |
Last edited by: Amit_86 at: 5/26/2014 11:59 PMLast edited by: Amit_86 at: 5/26/2014 11:56 PMVANDE MATARAM..... |
|
5/27/2014 12:15 AM | |
Posts: 133 Rating: (0) |
sorry, i can't find that. Could you please help me with coloured screen shot ? |
5/27/2014 6:50 AM | |
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181) |
Let's start with creating and downloading OBs.The following entry tells you which organization blocks do you need for error handling in the S7 program of the CPU:11499205. Then will discuss what is wrong there.
|
5/27/2014 9:10 AM | |
Posts: 133 Rating: (0) |
dearhdhosseini, Note that i am using PLCSIM in frensh, not english. thanks for the red card dearUMENCHO, I can't find "Options --> report system error"
|
Follow us on