Industry Online Support
Technical Forum
10/27/2014 9:42 PM | |
Posts: 32 Rating:
|
Welcome. I have a problem running PLCSIM with s7-1500. Every time I get an error as in the picture. |
10/27/2014 11:40 PM | |
Posts: 32 Rating:
|
I made the upgrade to version 5 update and it is still the same. |
10/28/2014 11:12 PM | |
Posts: 66 Rating:
|
Here is a PLCSIM project which contains a 1518-4 PN/DP. Try opening it in PLCSIM V13. You should be able to double click the project file after extracting, or in PLCSIM you can choose Project->Open and select the project that way. Note: If you try to open this sim13 project in PLCSIM V12, it won't work.
Attachmentdsout_sample.zip (60 Downloads) |
Follow us on