11/26/2017 10:39 AM | |
Joined: 12/18/2014 Last visit: 11/4/2024 Posts: 34135 Rating: (4254)
|
A factory reset is not possible with the 0BA8.Standard (FS: 02). This is only possible from the LOGO! 8.FS4 (FS: 04). If the LOGO! is in operator mode, then the entry in the menu for switching is "Switch to ADMIN". Which process asks for the password? AttachmentLOGO! 8 Soft manual 0BA8 2014_06 pages 63+64.pdf (218 Downloads) |
Last edited by: ixo65 at: 11/26/2017 10:44:34 AM |
|
11/27/2017 12:48 PM | |
Joined: 9/23/2015 Last visit: 3/4/2024 Posts: 21 Rating: (2) |
Thanks. I will start a support request. |
Follow us on