Industry Online Support
Technical Forum
1/13/2010 1:26 PM | |
Posts: 2 Rating: (0) |
Dear, I am using the sm331 Analog card (6ES7 331-7KF0-0AB0) with four wire and two wire configuration. Now four channels are used for 2 wire and four channels used for 4 wire. I attached file ther is my present configuration for the channels. As removed the negative from terminal no 11 then 4 wire four channels are worked . And whn the wiring is as it is then 2 wire four channels are worked. Now i am in confusion what to do. Please send some solution so i can connect 2 wire and four wire in one card. Thaking You Vivek Thawkar Automation Division Attachment20100113_153032.pdf (82 Downloads) |
Last edited by: O_Moderator at: 1/13/2010 1:31 PMnew subject after splitting from /tf/WW/en/Posts/38925#top |
|
1/14/2010 9:52 AM | |
Joined: 4/24/2006 Last visit: 5/3/2024 Posts: 8632 Rating: (1148) |
Dear Vivek Thawkar, Here is a link to manual: SIMATIC S7-300 module data Please have a look at chapter 6.7 See figure 6-15 and the NOTE. Best regards, Wizard |
Follow us on