5/27/2020 4:01 PM | |
Joined: 1/16/2020 Last visit: 12/6/2023 Posts: 19 Rating: (0) |
|
5/29/2020 12:33 PM | |
Joined: 8/3/2009 Last visit: 11/18/2024 Posts: 14181 Rating: (1774)
|
Hello Only if you write the function for the Limits simultaniously together with the Values for the Life trend. But you cannot overlay something on the Trend, because it will pop into the foreground in Runtime. you could do this with F(x) Diagram also. but here also you have to write the Values for the limit Graph manually: LINK Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on