6/12/2011 1:14 PM | |
Posts: 103 Rating: (0) |
DEAR EXPERTS PLS TELLME WHAT MAY THE REASONS OF SF IN PM-E 24V DC |
6/12/2011 1:34 PM | |
Posts: 103 Rating: (0) |
IF THE +VE ,-VE AND FEEDBACK ARE SHORT ,IS THIS CONDITION CREATE THIS TYPE OF PROBLEM THANKS |
6/12/2011 1:37 PM | |
Joined: 7/2/2008 Last visit: 5/16/2024 Posts: 928 Rating: (306)
|
Hello veer,
The manual says"No parameter assignment or incorrect module plugged in. A diagnostic message is pending." Make sure it's the correct module in the correct slot. Unplug it and plug it again. It will be better if you can go online with SIMATIC Manager and go in hardware configuration window and point to the module and press Ctrl+D and see what's wrong. Best regards. H-H |
6/12/2011 2:17 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (270) |
Dear veer, if possible pl attach diagnostic buffer info. |
VANDE MATARAM..... |
|
6/13/2011 8:40 AM | |
Posts: 947 Rating: (45) |
Hi veer |
6/13/2011 5:22 PM | |
Posts: 947 Rating: (45) |
Hi What MLFB has PM-E? Can be burned fuse? |
Last edited by: gre_m at: 6/13/2011 5:26 PM |
|
Follow us on