1/14/2019 7:22 PM | |
Joined: 3/27/2008 Last visit: 4/27/2024 Posts: 1098 Rating: (137) |
The PM250 in regeneration will not be tolerated by the UPS. |
Tractor |
|
1/15/2019 8:03 AM | |
Joined: 3/2/2007 Last visit: 4/26/2024 Posts: 929 Rating: (5) |
the UPS is MGE Galaxy 6000 . could it cause some issue ? |
... thank you ... |
|
1/16/2019 8:54 AM | |
Joined: 5/22/2012 Last visit: 3/24/2022 Posts: 895 Rating: (67) |
With OFF2 the pulses to the motor would be disabled. So no energy comes from the motor back to the DC Link. |
Follow us on