11/6/2008 3:10 PM | |
Joined: 12/12/2005 Last visit: 3/17/2024 Posts: 180 Rating:
|
Hi I wonder if I have problem to make data exchange between two multi projects. First multiproject has two PN/DP CPUs and one CP343-1 they using S7 connection (IE) and GET PUT blocks. Second multiproject has some 343-1, 443-1 and 343-1lean CPs. Using ISO-on-TCP connection AG send and AG Receive blocks. This first multiproject has made about 18month ago and I remember we tried to do it by AG send and Receive, but somehow it doesn´t start to work. (second network is older)Both multiprojectsare in same IP area and physically in same network. I have read many threads and found that there might be problem if I try to data exchange between these two multiproject, so my question: Is it possible use AG send/Receive. second question: I also read about open TCP/IP connection, but it doesn´t open when this kind solution is right?https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=en&objid=25209116&caller=view -Heksu- |
"Beer is proof that God loves us and wants us to be Happy"-Benjamin Franklin |
|
Follow us on