2/2/2023 12:28 PM | |
Joined: 8/12/2021 Last visit: 11/12/2024 Posts: 332 Rating: (31) |
Hi AmolGaikwad! The instruction D_ACT_DP can be used to specifically deactivate and reactivate configured DP slaves/PROFINET IO devices. However, I think you have to specify the line to be disabled (X1 or X2 or both). You can find more info here. |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
2/2/2023 12:47 PM | |
Joined: 3/11/2019 Last visit: 11/8/2024 Posts: 1653 Rating: (304)
|
Dear AmolGaikwad, it is possible. As the coupler is used to connect two (or more) PLCs, D_ACT_DP should bei used in both PLCs if the coupler is physically not present. How do you enable and disable DP slaves and IO devices using the "D_ACT_DP" instruction?regards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to1 thankful Users |
Follow us on