Industry Online Support
Technical Forum
10/8/2013 6:10 PM | |
Joined: 12/11/2009 Last visit: 9/8/2022 Posts: 243 Rating: (4) |
Hi i want to send/receive data between two CPU315-2PN/DP by using pn/pn coupler but i could not find any example project? At following pdf page 37 there is a good example, but i could not find project.it's only picture. http://support.automation.siemens.com/WW/view/en/44319532 If you can find an example project about data exchange between two CPU315-2PN/DP without using pn/pn coupler, it will be better. I don't want to use profibus for data exchange at this project. |
Last edited by: O_Moderator at: 10/9/2013 10:31 AMlink corrected |
|
10/9/2013 9:31 AM | |
Joined: 4/24/2006 Last visit: 6/26/2024 Posts: 8694 Rating: (1160) |
Hello Osman_, Perhaps this link might help: how do you program the communication blocks FB63 "TSEND", FB64 "TRCV", FB65 "TCON" and FB66 "TDISCON" in order to use the TCP protocol for data exchange by means of the integrated PROFINET interface of an S7-300 or S7-400 CPU? Best regards, Wizard |
This contribution was helpful to3 thankful Users |
Follow us on