4/18/2015 3:42 PM | |||
Posts: 5225 Rating:
|
|
||
This contribution was helpful to
2 thankful Users |
5/12/2015 7:57 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi, for handling the coupler- communication you need to configurate, like William said, the PN/PN coupler separately in each of the two projects. The manual will help you: https://support.industry.siemens.com/cs/de/de/view/44319532/en chapter4 regards, |
FCK WAR! |
|
5/27/2015 12:13 PM | |
Posts: 33 Rating:
|
Hi mopS04, The chapter 4 from the mentioned manual provides handy information about the hardware configuration. Which is fine ,except that I'm having issues in knowing which logic should I use in order to send data located into a DB block to the partner CPU . The partner CPU has the attached hardware configuration. So I guess my question is - is it possible to send DB data (let's say DB4 ) to the IN128 bytes module as it is shown attached capture? Thanks Best regards aney_312 AttachmentCapture_PNPN.zip (794 Downloads) |
Last edited by: aney_312 at: 5/27/2015 4:48:16 PM |
|
5/29/2015 3:35 PM | |
Posts: 33 Rating:
|
Hi mopS04 , Much appreciated . Regards aney_312 |
7/7/2015 9:59 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating:
|
|
4/19/2016 1:23 PM | |
Joined: 4/21/2006 Last visit: 8/27/2024 Posts: 510 Rating:
|
New question published by Awaisq is split to a separate thread with the subject status = 8551. Best regards |
Follow us on