6/3/2013 12:35 PM | |
Joined: 4/24/2006 Last visit: 4/17/2025 Posts: 8954 Rating:
|
Hello, Are you using some Organization Blocks for error handling, see the following link: Which organization blocks do you need for error handling? Which organization blocks do you have to load into the CPU to ensure that the CPU does not go into the "STOP" status when a remote I/O fails? When you use the Organization Blocks, there might be more information in Diagnostic buffer Best regards, Wizard |
Follow us on