10/28/2014 8:08 PM | |
Posts: 101 Rating: (0) |
Hi Good day for you all, I have question about using pointer with FB and with FC. are there any restrictions should be taken into cosideration during deal with any of them?.i ask that because in the file i attached here i make FB and FC to make smalljob using pointer but the result was that FB is executed correct (gives the result).but FC does not give the right result.please see the attached pics. and you will understand what i mean.
Attachmentwonder.zip (203 Downloads) |
10/28/2014 9:05 PM | |
Posts: 79 Rating: (1) |
FC 5 is not excuted (not enabled) its being blocked by normally closed logical 1 (m50.1) in OB1. while FB12 is being excuted by OB1 |
10/30/2014 7:43 PM | |
Joined: 1/28/2009 Last visit: 10/26/2024 Posts: 6852 Rating: (1365)
|
Hello, I think similar question was discussed in the German conferences,read more here: FC mit IN-Parameter vom Typ String
I hope this helps, Hamid Hosseini |
10/30/2014 7:54 PM | |
Posts: 101 Rating: (0) |
thank you M.r hossieni any way but,sorry i understand nothing.
|
1/4/2015 7:26 AM | |
Posts: 5 Rating: (0) |
So, how can i access the complex data type (like string or array) outputusingthe pointer? thanks! |
Follow us on