Industry Online Support
Technical Forum
3/15/2011 9:47 AM | |
Joined: 10/3/2010 Last visit: 9/27/2024 Posts: 1562 Rating: (191) |
Is it possible that some Layer setting is the cause? Did you check everything related to the layer? 1. check the Layer-property of your polyline object 2. which layers are switched On/Off (see bottom "Layer"-toolbar) 3. in the dropdown list next to the above, which layer is selected to be the active layer? Moving an object to the back won't work for example if the layer of that object is the active layer while other parts of the screen are on a different layer (silly, I know but I had this in the past too). |
B r g d s , |
|
This contribution was helpful to1 thankful Users |
3/15/2011 10:40 AM | |
Posts: 17 Rating: (0) |
Thanks SteBo! that was the issue. I had the objects on different layers |
Follow us on