11/4/2010 11:18 AM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating: (102)
|
Hi You first problem (a and b) you only can solve (without script) with an internal Tag. Set in the picture window(pop up) the internal tag to a value and dynamize the display (p.E the letter) with Dynamic Dialog. With it you can assign for each value of the tagan other valuefor display (i.E. the letter). Your secound problem you sovle with the "direct connection..." at the event mouseclick of the button. Use as "Source" the constant "0" and as "Taget" in the"Current Window" the property "Display" regards cumulus |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
Follow us on