10/6/2016 2:50 AM | |
Posts: 305 Rating: (1) |
PORTOL V14 ,does it can program with S110、S120、SIMOTION ? |
10/6/2016 4:50 AM | |
Joined: 10/2/2013 Last visit: 5/6/2024 Posts: 339 Rating: (52) |
hello Tech Wing, you should refer this link https://www.industry.siemens.com/topics/global/en/tia-portal/software/Pages/default.aspx |
Technology is best when it brings people together,so we are here now :) |
|
10/6/2016 7:28 AM | |
Posts: 305 Rating: (1) |
the V14 has not S driver ... |
10/6/2016 7:59 AM | |
Posts: 305 Rating: (1) |
1、SCOUT is has TIA and no TIA two version . after the two can up to V4.5 ? is not , D425 how can to do ? one Windows can install SCOUT V4.4 、SCOUT TIA V4.5 ? |
10/6/2016 8:16 AM | |
Posts: 305 Rating: (1) |
i have a D425 , i use it test program . new software ,i worry D425 can not to do ! |