8/18/2011 3:01 AM | |
Joined: 1/28/2009 Last visit: 8/5/2024 Posts: 6844 Rating: (1365) |
Hi To be sure about addressing conflicts and other frquent programing flaws, upload your codes here! Also check the following discussion: (P) Positive RLO Edge Detection not function??
|
This contribution was helpful to1 thankful Users |
8/18/2011 3:59 PM | |
Joined: 5/27/2009 Last visit: 8/14/2024 Posts: 122 Rating: (8) |
Ok, this is the part in my code where i am triyin to use (P). inside HW_PumpTesysT (to detect a transition between manual mode or auto mode) this FB906 is called twice inside FB100. AttachmentCodigo_p.zip (191 Downloads) |
8/18/2011 5:31 PM | |
Joined: 1/28/2009 Last visit: 8/5/2024 Posts: 6844 Rating: (1365) |
Hi Check the modified version of your program. addressing is clarified, you can monitor the transition signals as you defined and determined in the attachment. Best regards AttachmentPOS.zip (189 Downloads) |
8/19/2011 8:00 PM | |
Joined: 1/28/2009 Last visit: 8/5/2024 Posts: 6844 Rating: (1365) |
Hi Did you check the addressesindividually be logic analyzer software such as THIS or a simple counter to check the transition positive edge? Best regards |
Follow us on