4/5/2020 6:36 PM | |
Joined: 4/2/2019 Last visit: 3/6/2024 Posts: 9 Rating: (0) |
Hello, I need small help. I have new CPU 315 -2 DP/PN and two cards (DI and DO). When I make program for START and STOP motor (this is my first program on new CPU) and try to download on PLC appear message like on picture below. Can some help me with this problem? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/06/2020 09:28:41New subject after splitting |
|
This contribution was helpful to1 thankful Users |
4/5/2020 7:03 PM | |
Joined: 9/27/2006 Last visit: 9/10/2024 Posts: 12282 Rating: (2683)
|
Hello Nemanja; What kind of memory card do you have in the CPU 315-2PN/DP? The MMC is essential as a repository of the Load Memory fpr the CPU, since that is where the programs are downloaded to. If you are missing the MMC and try to download, you will get a message like you have, error code 294:38. See this discussion on a similar error code:
How can you obtain an overview of the memory concept of SIMATIC S7-300 CPUs and C7 devices? https://support.industry.siemens.com/cs/ww/en/view/7302326 In your case look at the description of point 4, SIMATIC S7-300 CPUs and C7 Devices With MMC Bay, List of available MMC for S7-300 (FEPROM cards) 256 Kbyte FEPROM 6ES7 951-1KH00-0AA0 1 Mbyte FEPROM 6ES7 951-1KK00-0AA0 2 Mbyte FEPROM 6ES7 951-1KL00-0AA0 4 Mbyte FEPROM 6ES7 951-1KM00-0AA0 Hope this helps, Daniel Chartier |
Follow us on