9/8/2008 10:01 AM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
About mounting CBE20 read manual: Control Units and additional system components (GH1) About assign IP address: When you put Sinamics S120 with CU320 go on Control Unit - Configuration and you will see button IP address. And in this way after download you will put IP address into CU. regards |
9/8/2008 10:10 PM | |
Posts: 133 Rating: (13) |
If STARTER allows you to assign an IP address to a new CBE20 board please let us know. I have been using the Primary Setup Tool as described in the attachment for assigning the IP address to the board. As far as I know STARTER does not have a built-in configuration program (i.e. NetPro)like S7 or Scout to assign an IP address to a CBE20.
AttachmentCBE20.pdf (824 Downloads) |
Last edited by: Drives_Coach at: 9/8/2008 10:34 PM |
|
Follow us on