4/20/2012 11:34 AM | |
Posts: 270 Rating: (53) |
Well one way to decide that could be up to the sum of ratings & thanks that post have gotten ;] |
4/20/2012 11:51 AM | |
Joined: 9/1/2005 Last visit: 8/1/2024 Posts: 4104 Rating: (194) |
Dear Users, have you seen the Highlight Threadswithin the left navigation? This could be a little bit like "the post of the day". Our Experts got the posibillity to mark threads as very interesting. This thread are listed within the List. In the future we are planning an automatism. Highlight Threads will be selected by ratings and views too. But we have to wait a little bit for this feature. There are a lot of interesting discussions and new ideas that are published during a premium campaign. I'm asking for your understanding that during campaign we moderators couldn't think about each of them in detail. But be sure, all of this ideas are notated an we will discuss about all of them after the campaign. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
This contribution was helpful to7 thankful Users |
4/20/2012 1:16 PM | |
Joined: 5/28/2008 Last visit: 8/6/2024 Posts: 4515 Rating: (838) |
A very good idea and a very good answer from CS moderator. But I noticed that till now there is only one thread exist in highlight threads! I think that Experts should make more effort to select best threads to highlight. Have a nice day for all of you.
|
Ayman Elotaify |
|
This contribution was helpful to2 thankful Users |
4/22/2012 8:46 PM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (270) |
Dear Moderators, today there is no post under highlighted thread. I think we must have such kind of system in place called post of the day and there should be a separate link containing all such important post. I think after campaign we can think 4 such system which can lead to high quality post and increase more and more engagement of people with fourm. Also we can acknowledge person with certification if person delivers the such post ton often. I know that you people send an invitation to such member to become expert but something other then this if possible. You people reserved all the rights to implement new things.This is only suggestion. |
VANDE MATARAM..... |
|
Follow us on