Industry Online Support
Technical Forum
6/25/2009 6:40 PM | |
Joined: 7/2/2008 Last visit: 4/5/2024 Posts: 928 Rating: (305) |
Hello Lalit, The selection is through jumper and the rated input current is 2 A for 110VAC and 1 A for 220VAC Please download this manual. You will find all information you need there. Best regards. H-H |
6/25/2009 7:01 PM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835) |
Hello, The power supply input voltage is 120/ 230 VAC. It could be selected via a red selector switch in the front of the power supply. See the attached picture. If you have moved the selector upwords, it will be for 120VAC. Regards, |
Last edited by: Ayman Elotaify at: 6/25/2009 7:02 PMAyman Elotaify |
|
Follow us on