Industry Online Support
Technical Forum
9/2/2011 3:08 PM | |
Joined: 8/18/2009 Last visit: 2/22/2024 Posts: 541 Rating: (33) |
Dear Expert, In one my Project 1.CPU224,8KB User Memory;AC/DC/RLY,Onboard 14DI/O 2. SITOP EVP 150 230 V AC/24 V DC/6 A 3. EM223,DI8x 24VDC,DQ8x Relay for CPU22X 4.EM235,4AI,1AO; for CPU22X only I have Prepared Power Wiring Diagram & attached here Please tell me 1.MCB Rating are correct 2.Is it necessary individual MCB for each EM 235,EM223 AttachmentPower.pdf (94 Downloads) |
Rajkiran Patil |
|
9/5/2011 6:24 AM | |
Joined: 8/18/2009 Last visit: 2/22/2024 Posts: 541 Rating: (33) |
Thanks Greg, I have take Q2 1A instead of 10A,but why in datasheet mentioned wrong i.e. 10 A. |
Rajkiran Patil |
|
Follow us on