10/7/2024 12:16 PM | |
Joined: 3/14/2008 Last visit: 10/8/2024 Posts: 2109 Rating: (941)
|
Hi, The predecessor for insert position is used to handle the block order in runtime groups of the CFC. If you select a block and right click, you can set this option. What happens is that new blocks are inserted after this block in the runtime group order. |
If I could help you, you can use the RATE button. Thank you. |
|
10/8/2024 6:56 AM | |
Joined: 3/14/2008 Last visit: 10/8/2024 Posts: 2109 Rating: (941)
|
Hi, I made some print screens to show you what happens. Please find enclosed the zip file containing three printscreens. I hope this clarifies. PS: When you click on the darker green rectangle in the block, you jump to the runtime sequence editor where you can drag and drop blocks in the order you would like to have. It's also possible to optimize the runtime groups automatically. The system determines the correct order of blocks according to your CFC logic. AttachmentPredecessor.zip (10 Downloads) |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on