4/3/2018 9:51 AM | |
Joined: 5/16/2016 Last visit: 5/24/2024 Posts: 71 Rating:
|
Hi, Hope it´s ok I insert my own question regarding S7 configuration here. I was thinking about presenting an Int as decimal value in Desigo CC. As far I can see there is only the Real object that can present a decimal value? It´s quite common in integrations into the predecessor to Desigo CC that values are presented as Int values and then XX amount of digits are presented as the decimal. Best Regards ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/3/2018 11:32:49 AMNew subject after splitting |
|
Follow us on