8/12/2019 9:49 AM | |
Joined: 3/1/2018 Last visit: 5/8/2024 Posts: 1 Rating: (0) |
Dear All, Can anyone help me on configuration of a QFAxis for Pressure Profile control? I have configured a hydraulic axis for pressure control. However, I got the following Error once I run the pressure profile by “_runtimelockedforceprofile” or “_enableforcecontrolbycondition”. "30008: Link to a technology object necessary for this operation does not exist." On the other hand, I can control the same axis pressure by “_setforcecommandvalue” perfectly without any error. Is there any special settings have to be set? AttachmentError Image.docx (271 Downloads) |
Follow us on