5/8/2019 12:21 PM | |
Joined: 9/19/2009 Last visit: 4/27/2024 Posts: 458 Rating: (81) |
Hi Until the firts task is not finished don´t start again. If you want test, create a push button with a sleep function or loop with several seconds, whatever you like, you can use HMIRuntime.Trace to see it. Then create another button with another code and push it. As I said, with HMIRuntime.Trace or printf function you will see how it works. Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
5/8/2019 12:45 PM | |
Joined: 9/19/2009 Last visit: 4/27/2024 Posts: 458 Rating: (81) |
Hi By default, It is how WinCC works "The task will not run again until the first has completed." You can tested, and see it how it works... Please use HMIRuntime.Trace for VBS or printf for ANSI C Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
5/8/2019 7:47 PM | |
Joined: 9/19/2009 Last visit: 4/27/2024 Posts: 458 Rating: (81) |
Hi I never experimented this situation, and I have tested with cycle 500ms and a few hundres of lines the code. However, you can check with TaskManager to see if the CPU go to 100%. Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|