2/5/2018 2:54 PM | |
Joined: 12/18/2014 Last visit: 10/6/2024 Posts: 33883 Rating: (4215)
|
With only 4 buttons, on each floor, how is this supposed to work? Describe the functional sequence. |
2/5/2018 3:08 PM | |
Joined: 12/18/2014 Last visit: 10/6/2024 Posts: 33883 Rating: (4215)
|
And what should happen if someone has pressed the PB4 and the lift has arrived at stage 4? |
2/5/2018 6:18 PM | |
Joined: 12/18/2014 Last visit: 10/6/2024 Posts: 33883 Rating: (4215)
|
In attachment a possible solution. The limit switches are NC. AttachmentLift_with_4_floors_LOGO!8.FS4.zip (283 Downloads) |
This contribution was helpful to1 thankful Users |
2/6/2018 10:16 AM | |
Posts: 42 Rating: (5) |
Hello ixo 65, thanks for your reply. the program is not getting opened in LSC V8.1 . And well my limit switches are NO. |
2/6/2018 10:38 AM | |
Joined: 12/18/2014 Last visit: 10/6/2024 Posts: 33883 Rating: (4215)
|
I created the program with LSC 8.1.1 and selected a LOGO! 8.FS4 hardware. Do not understand that you can not open them. Have now changed the hardware to 0BA8.Standard and saved the program with LSC V8.0. I changed the limit switches to NO and additionally created a message text. AttachmentLift_with_4_floors_0BA8.Standard.zip (280 Downloads) |
This contribution was helpful to3 thankful Users |
Follow us on