12/9/2015 2:04 PM | |
Posts: 26 Rating:
|
Hey, I have a problem with the configuration of my CU320-2 PN in Simotion Scout. If I search for accessible nodes, I can see my PLC CPU319 PN/DP and my CU as Bus nodes, but the CU should be a Drive Unit, whereby I can't place it in my project. If I go to the HW of my PLC and go online, I can see in the Module Information of the PROFINET, that my laptop and CU are connected but the CU is crossed. The Ethernet-cable is placed in the X150 P1 port of the CU Simotion Scout version: V4.4.0.2 Thank you attached a printscreen from the HW in the PLC and from the Bus nodes in Simotion
Attachmentprintscreens CU Error.rar (39 Downloads) |
12/10/2015 8:11 AM | |
Posts: 26 Rating:
|
Hello, I have installed the SSP with Safe mode with command prompt because the path name was to long, but it stil doesn't work. Regards, Jeroen |
12/10/2015 9:17 AM | |
Posts: 26 Rating:
|
Hi, I will try this, but I have a new problem now. I can't even download my HW from Step 7 to my PLC, but I can ping.. Regards, Jeroen |
Follow us on