Industry Online Support
Technical Forum
6/18/2019 3:14 PM | |
Joined: 4/28/2015 Last visit: 8/30/2022 Posts: 5 Rating: (0) |
Hello Cannot backup a specific segment. This problem was discovered when the server did not go into mode 'Active' (Active(Recovery)) after automatically creating a backup segment. MaintenanceService.exe took the maximum memory size (12 GB). (SQL TempDB.mdf> 30 GB) Disabled automatic creation of backups of segments. In manual mode, starting the creation of a backup of this segment led to the same situation. When creating a backup of other segments, everything is fine. How to fix this problem? How to disable a bad segment through SQL MS? PCS 7 v.8.0 SP1 ProcessHistorian 2013 Upd 6. AttachmentMaintenanceService.diagnostic.log.2019-06-19.1.txt (76 Downloads) |
Last edited by: AutoGen_1023725 at: 06/19/2019 08:06:17Backup arcive segment (100171) failed! Last edited by: AutoGen_1023725 at: 06/19/2019 08:18:02Last edited by: AutoGen_1023725 at: 06/19/2019 08:18:35 |
|
6/19/2019 1:47 PM | |
Joined: 4/28/2015 Last visit: 8/30/2022 Posts: 5 Rating: (0) |
Here is another part from the previous MaintenanceService.diagnostic.log.2019-06-19.0 (Full log size> 1 GB)
AttachmentError_BackUp_seg100171_20190619.txt (114 Downloads) |
Follow us on