Industry Online Support
Technical Forum
10/31/2007 2:59 PM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating:
|
Hello GOLD, Which OP7 panel do you have? What controller did you programm? Best regards, Wizard |
10/31/2007 3:13 PM | |
Posts: 5 Rating:
|
The program which i use, is the PROTOOL. I tried to transfer data from the project of prottol to the panel OP7-DP GOLD |
10/31/2007 3:21 PM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating:
|
Hi, look to this FAQ => http://support.automation.siemens.com/WW/view/en/13904923 USB -> seriell are not possible! regards, |
10/31/2007 3:24 PM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating:
|
Hello GOLD, You are using an USB - RS232 convertor. Unfortunately this will not work Best regards, Wizard |
10/15/2009 9:00 AM | |
Joined: 4/24/2009 Last visit: 7/18/2024 Posts: 2682 Rating:
|
Thread closed, because question is already discussed inthese threads WinCC Flexible OP7. Connect OP7 <-> PC(USB) via converter RS232<>USB. CANNOT DOWNLOAD PROGRAM FROM LAPTOP TO OP3. Simatic OP 27 and PC. Please continue to discuss in the last mentioned thread. Best regards O_Moderator |
Follow us on