4/3/2018 5:44 PM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
Hello, and which error occur? Christoph |
4/4/2018 8:13 AM | |
Posts: 64 Rating: (0) |
After downloading , i got on this information: Warning : 1903: COMM INT Warning : 1902: PB/PN : clock cycle..... D425 OK if i make "control panel" for axis , i got on : 30002 Command aborted sometimes : Error outgoing (Q). |
4/4/2018 9:06 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
please make screens and attach the diagnostic buffer! |
4/4/2018 9:22 AM | |
Posts: 64 Rating: (0) |
Thank you much to your reply.. Attached some pictures.. Attachmentpic.zip (83 Downloads) |
4/4/2018 9:29 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
Hello, ok reason 4 means that something is wrong with the profibus time settings. Which TI / TO you configure for the integrated?
Christoph |
4/4/2018 12:42 PM | |
Posts: 64 Rating: (0) |
attached config of TI/TO what is (p112ff) ? |
4/4/2018 2:58 PM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
Hello, p112/p110 are parameters on the drive. open the expertlist online and check this parameters. it can bew that the system has a sampletime of 250µs then the Ti is to low.
Christoph |
Follow us on