2/18/2016 7:58 AM | |
Joined: 8/26/2013 Last visit: 7/20/2024 Posts: 35 Rating:
|
Hello, Sir, Now I have moved to MCC programming i.e. to control two motors using MCC (not from Control panel of Axis or Drive). While following a video tutorial "SIMOTION SCOUT TIA Getting Started", I have gone through slide bu slide. Following errors occured when I do save & compile the project. Also when I do Ckhech Consistency. Screen shots attached for your guidance please. How to do next? AttachmentScreen shots.zip (157 Downloads) |
2/18/2016 11:48 AM | |
Joined: 8/26/2013 Last visit: 7/20/2024 Posts: 35 Rating:
|
Thanks for your guidance. Project is compiled & downloaded to the system successfully. But after doing all the requirements given in the video tutorial as mentioned earlier, the motors not moving using MCC logic. Also, I monitor MCC step by step, but no movement of motors. How to do next? Also, SF led flashing Red (slow, 0.5 Hz) My complete project is attahched AttachmentMCC_1.zip (145 Downloads) |
2/18/2016 12:05 PM | |
Joined: 5/12/2006 Last visit: 7/25/2024 Posts: 22324 Rating:
|
Hello, and where is the program stoped or not functional? you should out the repeat until for the LineModule not on the End of the program, put it on the beginning! If the Linemodule is not activated the enable for the axis is not working and so the move also not working! Update: attach modified prrogram Regards Christoph AttachmentMCC_2.zip (158 Downloads) |
Last edited by: ChristophD at: 2/18/2016 12:07:34 PMLast edited by: ChristophD at: 2/18/2016 12:32:15 PM |
|
Follow us on