2/17/2021 2:02 PM | |
Joined: 9/28/2017 Last visit: 3/9/2023 Posts: 5 Rating: (0) |
Hi All, I have a problem with information server 2014 SP3 OS : Windows server standard 2016 What can be the problem? |
2/23/2021 2:59 PM | |
Posts: 198 Rating: (60) |
Hello Laurens32, The issue looks quite strange as it is happening during the setup phase. Similar errors were found with respect to the SQL compatibility with the IS version, issues with IIS or issues with the respect to the setup frame. Considering this issue is difficult to troubleshoot with a single screenshot, it is better to raise a technical support request to get a quicker resolution. |
Last edited by: TechnoBlaze at: 02/23/2021 15:02:15 |
|
3/11/2021 9:04 AM | |
Joined: 9/28/2017 Last visit: 3/9/2023 Posts: 5 Rating: (0) |
Problem is solved with re-installation. |
This contribution was helpful to1 thankful Users |