11/4/2021 6:44 PM | |
Joined: 2/17/2020 Last visit: 9/26/2024 Posts: 1068 Rating: (192) |
Hi pet.arrrrr, Welcome to the forum! Is there any other instance of SQL database installed on the PC? If so, please follow this FAQ and try the individual installation of SQL Server 2016 SP2 again. In case it does not work, or if you do not have another SQL instance installed... maybe it would be better to start from a clean PC image and install WinCC from scratch. |
A rating will be well appreciated. |
|
This contribution was helpful to1 thankful Users |
Follow us on