4/13/2016 3:52 AM | |
Posts: 90 Rating: (0) |
Solved again buy the great Hugs! |
4/14/2016 8:47 AM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (819) |
Hello, maybe I will be try on PG/PC simple USB Wifi antena (replacement of your wrong Netw Adapter). Another device (some old Wifi router with Ethernet ports is probably enough) is configured like simple network. To that router you can plug your RJ45 cable from S7-1200. You must configure that router like prepare Wifi to network connection as simple Ethernet network, I think that this looks like simple connection but without wires On PG/PC interface you only select right Wifi adapter (USB dongle) and I think that this must work. Try it and give info. This was only quick idea to solve your problem, I think some free this type routers are common and available on companies, ask to your IT division for test. Update: maybe yes that USB-Ethernet adapter, but I was think about some like this: http://www.bestbuy.com/site/networking/wireless-usb-adapters/abcat0503007.c?id=abcat0503007 Then you can also sit in Office everywhere not only where wires are located. |
Last edited by: Duris_I at: 4/14/2016 9:02:28 AMLast edited by: Duris_I at: 4/14/2016 9:04:38 AMWith best regards... |
|
Follow us on