1/31/2009 4:18 PM | |
Posts: 6 Rating: (0) |
hello CBo i want manual of simatic logon compatibility with pcs7 6.1 sp2 if u have that link plz send me Regards Sagar1 |
Last edited by: sagar1 at: 2/1/2009 1:50 PM |
|
2/19/2009 2:03 PM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating: (102)
|
Hello sagar1, it is a little bit difficult which version is released for pcs7. In the following entry you can read: http://support.automation.siemens.com/WW/view/en/23234216 SIMATIC WinCC (when using SIMATIC Logon together with SIMATIC WinCC) |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
2/19/2009 2:58 PM | |||
Joined: 4/5/2006 Last visit: 12/3/2024 Posts: 917 Rating: (63) |
Hi sagar1, I downloaded
and read readme file (in attachement), it says in chapter 4: 4 Software Requirements 4.1 Operating Environment .... Using SIMATIC Logon together with WinCC SIMATIC Logon V1.3 incl. SP1 requires at least WinCC V6.0 including SP3 including HF1 or a newer version. from manual should be works with PCS7 v6.0SP2 too. Attachmentsl-readme.zip (106 Downloads) |
||
Follow us on