2/28/2012 1:14 PM | |
Joined: 3/14/2008 Last visit: 2/5/2025 Posts: 2167 Rating:
|
Maybe it has to do with your process image definition. (PIP1-15).Which is connected to your digital input card where the pulse is coming in? You have to check which process image partition is allocated to OB32 (<100ms). |
If I could help you, you can use the RATE button. Thank you. |
|
4/23/2012 7:31 AM | |
Joined: 3/14/2008 Last visit: 2/5/2025 Posts: 2167 Rating:
|
Hey chicken, Good that you solved your problem... Couldn't you see on module diagnostics about the faulty signal? Did you connect the parameter QBAD of drive block to a specific block? I'm asking because such a problem should be detected easily.... |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on