6/2/2015 1:01 PM | |
Posts: 2 Rating:
|
I also have the same problem but with 32 bits Windows 7. The version PLC is V4.1 with S7-1214C. The IP PLC is 192.168. 0 .1, I think that IP isn't the problem. Please I need a solution.
------------ |
Last edited by: josep77 at: 6/2/2015 1:03:40 PMLast edited by: CS Moderator at: 6/3/2015 11:37:35 AMsplitting |
|
6/6/2015 9:18 AM | |
Posts: 2 Rating:
|
In Tia Portal V13 it was disponible.But in Tia Portal V13 SP1 Is not disponible the interfaz S7-1200/S7-1500. You can see my screen picture. Thanks. |
6/6/2015 8:42 PM | |
Joined: 5/12/2006 Last visit: 7/17/2024 Posts: 22317 Rating:
|
Hello, it looks that the PLCSIM V13 installation is not correct. Or try the Registry settings which provided in the Thread:
Regards |
This contribution was helpful to
1 thankful Users |
Follow us on