11/2/2018 12:28 PM | |
Joined: 4/12/2018 Last visit: 6/29/2022 Posts: 4 Rating:
|
Hello sir, I am installed for TIA PORTAL V13 UP 6 BUT SIMATIC HMI KTP700 BASIC UPLOAD PROGRAM AT A TIME MASSAGE FOR ACTION CANCLED BEFORE UPLOADING DEVICE WHAT IS PROBLEM AND I AM UPLOAD FOR LAN WIRE ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/2/2018 5:14:20 PMNew subject after splitting |
|
11/2/2018 8:07 PM | |
Joined: 9/21/2012 Last visit: 4/6/2025 Posts: 4362 Rating:
|
That usually means that you just can't upload the program form the HMI to PG. It's very rare that the original programmer has enabled backtransfer. |
11/5/2018 8:10 AM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating:
|
Hello, what is the error message? can you post a screenshot?
|
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
11/14/2018 9:56 AM | |
Joined: 8/3/2009 Last visit: 4/4/2025 Posts: 15194 Rating:
|
Hello @ Hati that is not the Point in this case.... A Backtransfer is not possible in TIA Portal. --> Often the Words "upload" and "download"are used in the wrong context or people do not understand it without doubts. We should use the words "load to the Panel" and "loading from the Panel" then everyone knows what you mean. @ parmar ripal: check the Image Version of the Panel and compare with the Image Version in your Project. If its not equal then you have to do a OS Update first. In some Versions and situations the TIA Portal cannot do it automatically. in this case you have to do it manually first and then try to Load the Runtime Files to the Panel again. Here are some Basic FAQs: https://support.industry.siemens.com/cs/ww/en/view/58522603 https://support.industry.siemens.com/cs/ww/en/view/88633853 Bye Murof |
If this Information really helps, you could use the Rate function |
|
5/10/2020 12:19 PM | |
Joined: 4/12/2018 Last visit: 6/29/2022 Posts: 4 Rating:
|
|
5/10/2020 1:50 PM | |
Joined: 5/12/2006 Last visit: 4/4/2025 Posts: 22607 Rating:
|
no solution! transfer from panel to engineering not possible! |
5/10/2020 5:00 PM | |
Joined: 7/5/2013 Last visit: 4/4/2025 Posts: 3144 Rating:
|
Hello parmar ripal,
referring to Murof's post, which way do you want to load?
As Christoph mentioned, loading the project from the panel is not possible. If you want to load to the panel, then share some screenshots of your problem. Regards, Frink
|
Pi is exactly three! |
|
We are working on a new user interface with better overview and more relevance.
To explore the new Forum, you can follow the textbox in the right column, which will lead you to the corresponding page in the new Forum. Alternatively, you can start from the main page by following this link:
https://sieportal.siemens.com/en-ww/support/forum
In the coming days, we will update the configuration step by step, so that you are directed to the new Forum by default. The “classic Forum” will remain available for all known functionalities alongside the new one.
We are thrilled to finally share the future of our Forum with you. Thank you for your commitment!
Kind regards,
the Forum Support Team
Follow us on