Industry Online Support
Technical Forum
10/16/2012 1:12 PM | |
Posts: 8 Rating: (1) |
Hi all, I replaced old S5 module, analog input module 6ES5 466-3LA11 with follow-up anal;og module, 6ES5 466-4UA11 along with its recomended front connector and adjust all pin assignment as well as the hardware setting (switch setting), but the new module still cannot run. Here I attached my switch setting for both modules. The CPU is S5-115U with IM306 module. I read in 466-4UA11Product Information: ( http://support.automation.siemens.com/WW/llisapi.dll/csfetch/4204219/PI466E.PDF?func=cslib.csFetch&nodeid=4204224 on page 7 ) there is no support for with IM306 Expansion Unit (EU). The EU that supported are, IM304/314, IM307/317, IM308/318-3, IM300/312. Is it right that analog module 466-4UA11 incompatible with IM306? I still confuse how to set switch setting S9 and S3 for 466-4UA11. any help would be greatly appreciated. Thank you very much. AttachmentSwitch Setting 466-4UA11.pdf (379 Downloads) |
10/16/2012 4:33 PM | |
Joined: 1/30/2007 Last visit: 6/3/2022 Posts: 262 Rating: (24)
|
Hi andrian, where is the new analog module placed, central or extended rack? Good luck |
10/16/2012 7:12 PM | |
Posts: 8 Rating: (1) |
Hi Simaticus, it is located on extended rack , beside Power supply , some analog cards and in the end there is IM306.
|
Follow us on