Industry Online Support
Technical Forum
11/18/2013 5:03 AM | |
Joined: 4/11/2013 Last visit: 2/14/2025 Posts: 11 Rating:
|
We retrofiteando with sinumerik 840Dsl. The ALM is set up with "network control contactors sinamics Output terminal feeding contactor control "X132.12" contactor input terminal network response "X132.4". drives are configured. test the circuit. is observed that the contactor is not energized X132.12 terminal, the terminal X132.4 feedback all the time is "1" 700200 alarm time checkback feedback exced time it takes to acomplete sequence energized. thanks for your help Attachmentla%20foto.pdf (75 Downloads) |
Follow us on