Industry Online Support
Technical Forum
2/24/2014 12:22 PM | |
Posts: 1368 Rating: (126) |
Hello, the first thing: A FW update would often be helpful http://support.automation.siemens.com/WW/view/de/68042849 The SCALANCE S612 has no own Webserver (like SCALANCE X). So no Webbased Management is available at the Security modules.The configuration is made via Security Configuration Tool. If you want to reach the SCALANCE S via SCT, you need a project and the login-data for SCALANCE S(Username/Password). If you can not ping the SCALANCE S, it could be possible, that the firewall blocks ICMP packets. If you want to communicate to a module BEHIND the SCALANCE S via https/ VPN,make sure that the security modules involved have the current time of day and the current date. Otherwise the certificates used will not be evaluated as valid and the secure communication will not work Greetings |
2/25/2014 1:03 PM | |
Posts: 1368 Rating: (126) |
Jepp, this is the latest firmware. |
2/25/2014 1:17 PM | |
Posts: 7 Rating: (0) |
Pittiplatsch, thank you very much |
This contribution was helpful to1 thankful Users |
Follow us on