7/1/2015 8:55 AM | |
Posts: 4 Rating:
|
Sir, I am facing the problem with accuracy of measurement of water levels. It shows very high reading sometimes. Sensor is mounted correctly...not to tight or other problem....water is also steady without spikes. Weir construction is also perfect. Sensor works perfectly, when we test it other places. I think...some ultrasonic interference could be there....but not sure..... Please give the possible reasons for such problem....and possible solutions.... Thanks ---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 7/1/2015 1:13:40 PMNew subject after splitting |
|
7/2/2015 2:50 AM | |
Joined: 3/28/2010 Last visit: 12/1/2023 Posts: 987 Rating:
|
The January 06, 2015 issue of European Automation ran the article The Top Five Things that Cause Inverter Failure. The 5th reason cited is ultrasonics that are generated inside the drive: http://www.euautomation.com/uk/automated/article/the-top-five-things-that-cause-inverter-failure AttachmentNoise issues - ultrasonics, pp from LUT400 manual.pdf (153 Downloads) |
This contribution was helpful to
1 thankful Users |
7/13/2015 11:29 AM | |
Joined: 12/13/2012 Last visit: 10/5/2023 Posts: 124 Rating:
|
There is also a noise guide available to prevent the noise. It´s not the latest one. The LUT is not mentioned here. Anyhow, the LUT400 is similar to the Multiranger 200.
Cheers AttachmentLevelguide_ultrasonic_en.pdf (156 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on