Industry Online Support
Technical Forum
9/28/2006 6:16 PM | |
Posts: 8 Rating:
|
Thank you for your reply, Nemo. Apparently the two tags have the same size, as I can see in the Runtime Simulator (FFFFFFFF in hex is the maximum value) and in the Script Debugger. Indeed, I can't choose LONG64, INT64 or DWORD64 in WinCC Flex. I'm using a Pentium IV 3'0 GHz 32 bits. Might it be a bug? It's rather strange. |
Follow us on