2/11/2010 10:39 PM | |
Joined: 10/17/2007 Last visit: 7/14/2024 Posts: 4008 Rating: (353) |
Hi, what is your PLC program for Communication.? Attachment611U_PZD.zip (344 Downloads) |
If you like my comments please |
|
2/12/2010 2:19 PM | |
Joined: 2/10/2010 Last visit: 11/21/2023 Posts: 35 Rating: (0) |
Dear nulizhang, thanks for support Unfortunately I have not any visible progress on my task. Once again, environment of my problem is as follows. I have loaded the project 611u_39 with Function Block FB 83 from SIMODRIVE 611U 12.2 Package/toolbox_120101. It was loaded correctly to controller and truly executing by the CPU. My question: How can I test the Profibus working cycle process? For clarity: HW Config (see attachment), Profibus parameterization (see attachment), drive configuration (see attachment). After SimoComU starting the message "831: Profibus is not in data transfer condition (Warning)" is still appearing. Is it enough what I have in my project for correctly Profibus working? You wrote: (I can only give your a tip to try. if it works post some feed back info. you can check manual 611U from DoconWeb. in Ch. 5(see attach.) set bit 10="1"). I have read a manual 611U, and its chapter 5. Sorry, I am beginner at S7 300/Simodrive.. So, I don’t know how to set bit 10="1" in STW1. Please tell me some kind of instruction. AttachmentConfig.zip (289 Downloads) |
2/12/2010 8:11 PM | |
Joined: 10/17/2007 Last visit: 7/14/2024 Posts: 4008 Rating: (353) |
Hi, Max 1) check attachment. you should get the diaplay like in my picture when you highlight SIMODRIVE 611U IN S7 HW config. (profibus) hten copy your picture post to me, i will give you more tips. 2) you should read Ch5. more carefully BR Attachment611u_config.zip (280 Downloads) |
Last edited by: nulizhang at: 2/12/2010 8:17 PMIf you like my comments please |
|
2/13/2010 2:54 AM | |
Joined: 2/10/2010 Last visit: 11/21/2023 Posts: 35 Rating: (0) |
Hi, nulizhang I get you my display with SIMODRIVE 611U in S7 HW config (attachment). Thank you for your help. AttachmentHW 611 config.zip (277 Downloads) |
Follow us on