8/9/2017 8:12 PM | |
Joined: 11/20/2013 Last visit: 8/27/2024 Posts: 25 Rating: (1) |
Hello I'm facing similar problem with CPU414-4H and did a firmware update to 4.5.7, Checked all the pins of UR-2H rack and grounding of rack. But the problem is not solved. After the firmware update the problem reappeared in about 15 days and I managed to collect diagnostic buffer information but I don't understand what is the cause to the problem. I'm attaching the diagnostic buffer herewith can you or anyone please explain where from this "defective" message is triggering? PS: I also faced this same problem with CPU417-5H where I had to replace the CPU and last night for the first time with 319-F. I'm attaching the diagnostic buffer information of both the CPUs. ------------------------------------------------------------------------------------------ AttachmentFaultyCPU.zip (303 Downloads) |
Last edited by: Jen_Moderator at: 8/10/2017 7:59:42 AMNew subject after splitting |
|
Follow us on