8/7/2008 9:07 AM | |
Posts: 102 Rating:
|
Hello John!!1 I am not familiar with the omron software, however here is the link where you can find the gsd files. https://support.automation.siemens.com/WW/llisapi.dll?aktprim=0&lang=en&referer=%2fWW%2f&func=cslib.csinfo&siteid=cseus&caller=view&extranet=standard&viewreg=WW&nodeid0=10805299&objaction=csopen or https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&lang=de&objid=6ES7153-1AA03-0XB0&caller=view the last one is in german just go to Downloads - Profibus GSD - Dateien Is this information useful?? |
8/7/2008 11:17 AM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating:
|
Hello, The new 1.25 version of the GSD is a more sofisticated one with support of extended User parameter data. I would try with the basic GSD 1.21. May be you will loose some feartures, but it is better than no communication at all I put it in annex AttachmentIM153-1_default.zip (348 Downloads) |
Best regards |
|
8/8/2008 1:56 PM | |
Posts: 4 Rating:
|
Hello , I usedsiem801d.gsdV1.21 IM153-1 DEFAULTthen I set the parameters according to the attachedPDF . but no result !! I am getting the same error. Best regards AttachmentIM153-1.pdf (283 Downloads) |
8/8/2008 2:41 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating:
|
Hello, There are several versions of Profibus DP (due to enhancements and new features in the standard evolution). The firts was DP Than we get DPV1 (DP version 1, with extra parametrazation possibilities during operation, acyclic read and write ofrecords, ...) In the mean time DPV2 is also available but concerns mainly isochronous mode, slave-to-slave cross communication. Important is to know what the master supports. DP, DPV1? The PDF you showus is for DPV1. For DPV1 you have the GSD Station type: ET 200M (IM 153-1) DPV1 Order no.: 6ES7 153-1AA03-0XB0 Version: V1.6 (12/2007) To be downloaded at the link: http://support.automation.siemens.com/WW/view/en/113498 |
Best regards |
|
Follow us on